PSG/Blackmer Pumps

Properly Aligned

Sometimes one good idea can change everything. This was the case when NORD approached PSG, a Dover company, with a design alternative that would greatly improve its Blackmer product line. In fact, this engineering innovation is so effective that the then potential customer is now a NORD business partner and has made plans to incorporate the concept into all of its Blackmer GNX Series pumps.

Solving the Coupling Challenge

"The industry has been living with the challenge of coupling alignment for as long as there have been electric pumps," PSG product manager, Geoff VanLeeuwen said. "As competition grows and skilled technicians become increasingly scarce, those responsible for plant operations often settle for a quick “eyeball it as best you can” approach to shaft alignment, accepting the fact that pump life will suffer as a result.

“Companies need to make money,” VanLeeuwen continued. “In a typical chemical plant or rail terminal, for example, you could be facing hundreds of dollars per hour in lost productivity if a pump goes down, and possibly far more than that. So they’ll do whatever it takes to get it up and running quickly. The problem is that poor maintenance has a snowball effect. Instead of spending a couple hours to properly align a pump, suddenly you have a day or two of unexpected downtime when the coupling fails or the pump seizes, just because someone was rushed. Our new GNX alignment-free pumps eliminate all that.”

The new Blackmer products utilizing NORD's hollow shaft design also make the installation process much easier. "Because it is basically plug and play, the amount of integration work required by the customer facility has pretty much dropped to zero," VanLeeuwen said. “So instead of 15 percent of our pumps being sold as turnkey solutions, that figure increased to 72 percent last year, which comes out to a net revenue improvement of 47 percent.”

PSG is just getting started. The first phase of their Blackmer GNX- and GNXH-series rollout – now complete – focused on its 2- and 2.5-inch flange pumps. Using a NORD SK 771.1 gear unit directly coupled to a Blackmer heavy-duty, self-adjusting sliding vane pumps, the self-contained units offer maximum flow capacities of 86 gpm (325 L/min) and 155 gpm (587 L/min) respectively. Phases II and III (which VanLeeuwen expects will be completed over the next six months) will extend to the Blackmer larger frame 3- and 4-inch pumps, boasting up to 50 HP and 500 gpm (1,893 L/min).

Building on Success

NORD is also busy rolling out new products. Their single-stage, inline helical gear units (used with the Blackmer GNX- and GNXH-series pumps) will be expanded with three larger products – the SK 871.1, SK 971.1 and SK 1071.1. Each is available with NORD’s exclusive hollow-socket option.

Gear units from NORD are ideal for virtually any high-speed pumping, mixing, or conveying application. Unlike the aluminum alloy construction of the smaller single-stage products, the three new gear units feature solid cast iron housings.

NORD's output torques range from 3,540 to 8,850 lb-in. with gear ratios from 1.4:1 to 8.1:1 and a power range of 1.5 to 60 HP. Mounted by a choice of foot-mount, IEC flange-mount (B5 or B14), foot/flange mount, or NEMA standard output flange and shaft, these gear units provide the flexibility customers need to specify drive solutions for a wide range of applications. These new units replace NORD’s SK 41E and SK 51E and are interchangeable with other European-designed gear units.

These and other NORD gearboxes offer a long list of standard features, including a robust one-piece UNICASE™ housing, Autovent pressure regulation, and high-strength, high-precision carburized gearing along with high-capacity bearings.

For extreme shaft and bearing loads, customers have the option of upgrading to twin-tapered roller bearings and a higher-strength alloy steel shaft.

“What differentiates NORD from the competition are high-quality products, short lead times, and excellent customer support,” said Tom Koren, director of engineering at NORD. “We're probably not the least expensive supplier, but as illustrated in our relationship with Blackmer, our solutions are extremely innovative and we’re a good business partner.”

VanLeeuwen agreed, summarizing the relationship like this: “NORD was willing to dedicate time and resources to solve a specific problem faced by everyone in this industry.” He laughed. “The ironic part is we didn’t really invent anything. People have been using motors, gearboxes, and pumps for decades. What makes our solution so effective is the way we paired them together. It’s been so successful that we’ve decided to gradually phase out all of our own gear units in favor of NORD’s. As proven leaders, Blackmer and NORD offer the new industry standard for pump unit assemblies. It eliminates unexpected downtime, and simplifies installation and maintenance tasks. Plus, installations benefit from noticeable improvements in uptime and ease-of-use. Welcome to the new normal of pump reliability.”

Joining Forces

PSG and NORD initially had one goal – eliminate the one component that causes the greatest amount of grief in a typical pump drive application – the coupling. “For the previous five or six years, I’d been thinking about developing a hollow socket shaft design for our inline speed reducers,” Koren said. “So when we heard that PSG was looking at a redesign of its Blackmer sliding vane pump families, it was an opportunity for us to present the no-coupling concept of directly interfacing their pump with our speed reducer. They agreed to test it, and here we are today as their main gearbox supplier.”

PSG product manager Geoff VanLeeuwen said there were several good reasons to adopt the hollow socket design. “Anytime you have two mating shafts, they must be kept in alignment – if not, you end up with additional load and possibly vibration that will reduce the life of that product,” he explained. “The problem with a traditional pump and motor arrangement is that a coupling is used to join them. Even a skilled technician needs a fair amount of time to get the different pieces shimmed, tweaked and aligned properly. The effort is required not only during the initial installation, but also whenever routine maintenance is performed.”

NORDBLOC.1® Helical Inline Gear Motor

Quiet Operaton, Hygienic Design

  • Power: 0.16 HP - 50 hp (0.12 kW – 37 kW)
  • Torque: Up to 29,207 lb-in 30 Nm – 3,300 Nm
  • Wash-down capable, available with NXD tupH® for food-safe applications
  • Lightweight aluminum housing
  • Quiet operation

Related Products and Services